Omega.com - Your one-stop source for process, measurement, and control Omega Engineering 1-888-TC-OMEGA(US & Canada) 1-203-359-1660 (International)
HomeQuick OrderProductsFree LiteratureMy OmegaOmega Info
View Cart Help Contact Us
Back to omega.com
Panel Meters
 
   Introduction to Panel Meters



Product Links
View All Panel Meters
Temperature and Process Panel Meters
Totalizers
Large Displays
Multi-Input Indicators and Scanners
Benchtop Meters
Analog Meters
Timers and Counters
Benchtop Meters
Wall Mount Indicators
Panel Meter Selection Guide
Technical Links
OMEGA PT41 Precision
Clock/Timer/
Controller Functions

What is a Panel Meter? A panel meter is an instrument that displays an input signal in either a digital or analog form. Many panel meters also include alarm options as well as the ability to connect and transfer data to a computer. OMEGA's iSeries panel meters are available with an ethernet option which allows the panel meter reading to be accessed across a local area network (LAN) or even through the internet.

Standard Sizes
Since panel meters are generally mounted inside an instrument panel, the panel must be cut to accommodate the panel meter. In order to provide interchangeability between panel meters, most panel meters are designed to standard DIN sizes. The most common DIN sizes are shown below.
Standard DIN Cutouts for Panel Meters
DP116
Compact Temperature Meters: DP116
An economical 3/64 DIN panel meter that has a full size 0.56" green or red LED display, built-in analog output and display hold capability.
More details »


   Types of Chart Panel Meters
Temperature and Process Panel Meters
The most common types of panel meter is one that accepts a single input and provides a digital display of the signal. These meters typically accept inputs from temperature sensors such as thermocouples and RTDs as well as process signals such as 4-20 mA, 0-5 Vdc and 0-10 Vdc.

DP25B Series
Totalizers
A totalizer is a type of panel meter that provides a summation over time of the input signal. Totalizers are commonly used with pulse inputs to provide a count of the number of pulses. This is typically used in flow measurement applications.
DPF400
Large Display Panel Meters
Large display panel meters are commonly used when the display must be visible at a distance. OMEGA's ILD series features digits as large as 4 inches in height.
ILD Series
Multi-Input Indicators and Scanners
OMEGA offers several panel meters that can accept more than one input. Some meters can switch from one channel to the next by pressing a button on the front of the meter while others will automatically scan through a series of channels. OMEGA's CN612 can accept up to 12 temperature inputs.
CN600 Series
Benchtop Meters
OMEGA offers panel meters built into a benchtop case. The benchtop case provides portability and is commonly used in laboratory applications.
MCS Series
Wallmount Meters
For those applications where a panel is not available, OMEGA also offers wall mount indicators. The benchtop case provides portability and is commonly used in laboratory applications.
DP550
Analog Meters
At one time most meters were analog style, however, with the advent of digital technology analog meters have become rare. Analog meters are dial type gauges, like the speedometer in most cars. However there are some applications which still dictate analog meters.
7000 Series
Anemometers | Automation | Accelerometers | Calibrators | Cartridge Heaters | Chart Recorders | Cryogenics | Custom Pressure Transducers | Data Loggers | Data Acquisition | Dial Thermometers | Fiber Optics | Flexible Heaters | Flowmeters | Glass Bulb Thermometers | Grippers | Heaters | Humidity Measurement | Immersion Heaters | Infrared Thermometers | Level Measurement | Load Cells | Magnetic Flow Meters | Panel Meters | Pressure Gauges | Pressure Transducers | Rotameters | RTD | Remote Process Monitoring | Sanitary Sensors | Signal Conditioners | Stepper Motors | Strain Gages | Strip Heaters | Temperature Controllers | Temperature Labels | Temperature Measurement | Temperature Sensor Manufacturing | Temperature Transmitters | Thermal Imagers | Thermistors | Thermocouple | Thermocouple Wire | Thermowell | Ultrasonic Flow Meters | Wireless Sensors