Omega.com - Your one-stop source for process, measurement, and control Omega Engineering 1-888-TC-OMEGA(US & Canada) 1-203-359-1660 (International)
HomeQuick OrderProductsFree LiteratureMy OmegaOmega Info
View Cart Help Contact Us
Back to omega.com
Panel Meters
 
   Introduction to Signal Conditioners



Product Links
View All Signal Conditioners
Technical Links
What is a Signal Conditioner?

A signal conditioner is a device that converts one type of electronic signal into a another type of signal. Its primary use is to convert a signal that may be difficult to read by conventional instrumentation into a more easily read format. In performing this conversion a number of functions may take place. They include:
  • Amplification
    When a signal is amplified, the overall magnitude of the signal is increased. Converting a 0-10mV signal to a 0 -10V signal is an example of amplification.

  • Electrical Isolation
    Electrical isolation breaks the galvanic path between the input and output signal. That is, there is no physical wiring between the input and output. The input is normally tranferred to the output by converting it to an optical or magnetic signal then it is reconstructed on the output. By breaking the galvanic path between input and output, unwanted signals on the input line are prevented from passing through to the output. Isolation is required when a measurement must be made on a surface with a voltage potential far above ground. Isolation is also used to prevent ground loops.

  • Linearization
    Converting a non-linear input signal to a linear output signal. This is common for thermocouple signals.

  • Cold Junction Compensation
    Used for thermocouples. The thermocouple signal is adjusted for fluctuations in room temperature.

  • Excitation
    Many sensors require some form of excitation for them to operate. Strain gages and RTDs are two common examples.
OM8 Series
AC Voltage & Current Measurement Transducers: OM8 Series
Convert AC currents and voltages to DC process signals for direct connection to data acquisition and recording systems. The OM8 employ average measurement techniques in conditioning the AC signal.
More details »


   Signal Conditioners
DIN Rail Mount
As the name implies, a DIN rail mount signal conditioner mounts on a DIN rail bracket. DIN rail conditioners are very popular in industrial applications since they provide a rugged mounting format for either a few or a large number of signal conditioners.

DRG Series Din Rail Mount Signal Conditioner
Backplane Mount Conditioners
Certain signal conditioners can also be mounted on a common backplane. The backplane style provides the advantage of all output signals being accessible through a single common connnector. The backplane style signal conditioners are often used with data acquisition systems since a single cable can connect multiple conditioners to a data acquisiton device.
OM7 Series Backplane Mount Conditioners
Digital Signal Conditioners
Digital conditioners are one of the more recent developments in signal conditioners. The output of a digital signal conditioner is converted to a digital format such as RS232, RS485 or even Ethernet. Digital signals have several advantages over analog signals. They provide a high degree of immunity from electrical noise, they can also support extended transmission distances and are easily connected to a computer. With an ethernet output, the input signal can be read across an entire network or even across the internet if so configured.
D1000 Digital Signal Conditioners
Automation |Accelerometers | Calibrators | Cartridge Heaters | Chart Recorders | Cryogenics | Custom Pressure Transducers | Data Loggers | Data Acquisition | Dial Thermometers | Fiber Optics | Flexible Heaters | Flowmeters | Glass Bulb Thermometers | Grippers | Heaters | Humidity Measurement | Immersion Heaters | Infrared Thermometers | Level Measurement | Load Cells | Magnetic Flow Meters | Panel Meters | Pressure Gauges | Pressure Transducers | Rotameters | RTD | Signal Conditioners | Stepper Motors | Strain Gages | Strip Heaters | Temperature Controllers | Temperature Labels | Temperature Measurement | Temperature Sensor Manufacturing | Temperature Transmitters | Thermistors | Thermocouple | Thermocouple Wire | Thermowell | Ultrasonic Flow Meters

©2003-2009 Omega Engineering