Instructions for setup, using Java Runtime Environment 1.5 (5.0)
  1. Go to your computer's Control Panel. Open the Java Plug-in
  2. Click on "Settings" & "View Applets" in the "General" tab.
  3. Select the "Settings" button on the General Tab
    Un-check the "Enable Caching" box. Then close dialog box to show the General Tab again
  4. Select the "Network Settings" button on the General Tab.
    Proceed to the Browser tab.
    follow the BROWSER PROXY SELECTION instructions below.
    You should either select the "Use Browser Settings" option or the "Direct Connection" option depending on the network connections between your computer and the iServer product. (Generally, select "Direct Connection" if accessing iServers on your local network and select "Use Browser Settings" option for access from your internal network to the internet.)
  5. Refresh or restart the webpage.

Instructions for setup, using Java Runtime Environment 1.4
  1. Go to your computer's Control Panel. Open the Java Plug-in
  2. Select the "Cache" Tab
    Un-check the "Enable Caching" box
  3. Select the "Proxy" Tab
    follow these BROWSER PROXY SELECTION instructions below.
    (Generally, un-check the box if accessing iServers on your local network and check the box for access from your internal network to the internet.)
  4. Refresh or restart the webpage.


BROWSER PROXY SELECTION

Accessing iTHX units within your internal network

1. Usually when the computer and iTHX are on an internal network, you will not use Proxy server access.

2. You should un-check the "Use Browser Settings" option on the "Proxy" tab

Accessing iTHX units to the internet

1. Often the web browser will use Proxy server access to the internet. In such cases, the default Java runtime settings on the "Proxy" tab should suffice. The default setting is the "Use Browser Settings" option.

2. If the default proxy setting doesn't work, then you may have a situation where the proxy settings of the web browser are incorrect.

Diagnostics:

If the web page of the iServer appears, then the HTTP Proxy is working fine.

If the data isn't updated on the iServer upon selecting the Read Sensor web page, there may be a problem with access through a winsock proxy server. In such cases your network administrator will need to provide the winsock proxy server and port #s. (If the administrator requires knowledge of the port # required on the iServer, the value is 2003).

These values should be entered into the Socks line on the "Proxy" tab (of the Java Plugin control panel) or into the "connections" tab on the View,Internet Options dialog and make sure that the Proxy tab shows that the "Use Browser Settings" option is not selected (i.e. when you specify proxy connections in the Java Plugin control panel.

Accessing iTHX units over Peer-to-Peer network

A simple peer-to-peer network is setup by disconnecting from the main network (as users will often do when trying to do initial setup of the iServer) and then connecting the iServer to another computer using a ethernet hub, an ethernet switch, or a Cross-over cable connection.

Often when using a peer-to-peer network, the Java plugin and the web browser (such as Internet Explorer) have internet connections configured to connect through proxy servers. In such case, you will need to simply assign the final IP address on this peer to peer network and then view the iTHX charts after connecting the iTHX into the regular network. Otherwise you can disable the Java plug-in's "Use Browser Settings" temporarily and then reconfigure the Java plug-in settings for regular network access after testing the iTHX chart access on your peer-to-peer network.

The "Use Browser Settings" should not be selected. And the HTTP and Socks proxy entries should be blank. Also, setup the internet browser so that proxy servers are disabled.


If you still have problems viewing the DEMO and you are on a Proxy Server or are behind a Firewall, please contact your MIS administrator to verify that you have the lastest Proxy Client Software, version 2.0 or higher.

Java and the Java Coffee Cup Logo are trademarks or registered trademarks of Sun Microsystems, Inc. in the U.S. and other countries."