Omega.com - Your one-stop source for process, measurement, and control Omega Engineering 1-888-TC-OMEGA(US & Canada) 1-203-359-1660 (International)
Home Online Store Products Literature My Omega Omega Info Contact Us View Cart Help Global
Navigation Image Map   Help Icons image map
search
      
   


This page is from a previous version of the Omega.com site,
information and pricing may be invalid.


For TUBING, go to our current TUBING product listing.

For tube FITTINGS, go to the current Tube FITTING product listing.



 
Technical Information: Fluorocarbon Resin
Technical Section
Table 1
Typical Properties* of Fluorocarbon Resins

-
ASTM
Standard
Units

PTFE

FEP

PFA
Mechanical Properties:
Specific Gravity
D792
--
2.13-2.22
2.15
2.15
Tensile Strength
D638
psi
2,500-4,000
3,400
3,600
Elongation
D638
%
200-400
325
300
Flexural Modulus
D790
psi
27,000
90,000
90,000
Folding Endurance
D2176
(MIT) cycles
>10
5-80 x 10
50-500 x 10
Impact Strength
D256
Ft-lb/in.
3.5
No Break
No Break
Hardness
D2240
Shore D
50-65
56
60
Coefficient of Friction Dynamic
D1894
<3 m/min
<10 ft/min
0.1
0.2
0.2
Thermal Properties:
Melting Point
DTA,E-168
ƒC
(ƒF)
327
(621)
260
(500)
305
(582)
Upper Service Temperature (20,000 hr)
UL-746B
ƒC
(ƒF)
260
(500)
204
(400)
260
(500)
Flame Rating**
UL-94
--
VO
VO
VO
Limiting Oxygen Index
D2863
%
>95
>95
>95
Heat of Combustion
D240
Btu/lb
2,200
2,200
2,300
Electrical Properties:
Dielectric Constant
D150
1 Mhz
2.1
2.1
2.1
Dissipation Factor
D150
1 Mhz
0.0001
0.0007
0.0001
Arc Resistance
D495
sec
>300
>300
>180
Volume Resistivity
D257
Ohm-cm
10
10
10
Surface Resistivity
D257
Ohm/sq cm
10
10
10
General Properties:
Weather Resistance
Florida Exposure
Years Unaffected
20
20
10
Chemical/Solvent Resistance
D543
--
Outstanding
Outstanding
Outstanding
Water Absorption-24 hr
D570
%
<0.01
<0.01
<0.03
*Typical values are unsuitable for specifications. Properties were measured at 23ƒC (73ƒF), unless otherwise noted.
**Statements regarding behavior in a flame situation are not intended to reflect hazards presented by this or any other material when under actual fire condi
tions.

The following characteristics contribute to the unique properties of fluorocarbon resins:

• Nonpolarity–The carbon backbone of the linear polymer is completely sheathed by the electron cloud of fluorine atoms, much like a wire core is protected by insulation coating. This ensheathment, and the angles at which the carbon-fluorine bonds are disposed, causes the centers of electronegativity and electropositivity to be perfectly balanced across the polymer chain cross section. As a result, no net charge difference prevails. This nonpolarity of the polymer is partly responsible for its lack of chemical reactivity.

• Low interchain forces–The bond forces between two adjacent polymer chains are significantly lower than

the forces within one chain. PTFE linear polymer chains are otherwise restrained. However, in FEP and PFA, interpolymer chain entanglement of the pendant structure precludes the shifting of polymer chains to relieve the implied load. The ìcreepî normally associated with PTFE is mostly avoided with FEP and even more so with PFA.

• High C-F and C-C bond strengths are among the strongest in single bond organic chemistry. The polymer must absorb considerable energy to disrupt these bonds. Chemical reactions represent a kinetic and thermodynamic resolution of bond-making and bond-breaking in favor of the most stable system. These bond strengths are hard to overcome.
The data listed here fall within the normal range of product properties but they should not be used to establish specification limits or used alone as the basis of design. The DuPont Company and OMEGA Engineering, Inc. assume no obligation or liability for any advice furnished by it or for results obtained with respect to these products. All such advice is provided gratis and Buyer assumes sole responsibility for results obtained in reliance thereon.

and Tefzel are registered trademarks of The DuPont Company.

• Crystallinity–The high degree of crystallinity in these semicrystalline polymers results in high melting points, mechanical properties, and an integral barrier to migrating, small, nonpolar molecules. Under certain conditions, these molecules penetrate the plastics.

• High degree of polymerization– The unbranched nature of the polymers and their low interpolymer chain attraction requires very long chain lengths in PTFE and entanglement in FEP and PFA to provide load-bearing mechanical properties. The chain length also has an impact on flow and crystallinity of the polymers. These unique properties lead to the following benefits:

• High melting points (327ƒC [621ƒF] for PTFE; 260ƒC [500ƒF] for FEP, and 305ƒC [582ƒF] for PFA). The melting point of PTFE is one of the highest in organic polymer chemistry. Other materials can attain higher temperatures, but they degrade rather than melt. Compared to PTFE, the lower melting temperature of FEP results from lower degrees of polymerization and crystallinity. In PFA, a higher degree of polymerization, enhanced entanglement of the pendant structure, and lower comonomer content combine to provide a melting point closer to that of PTFE.

• High thermal stability–Due to the strength of the carbon-fluorine and carbon-carbon single bonds, appreciable thermal energy must be sorbed by the polymers before thermal degradation. The rate of decomposition of a part of depends on the particular resin, temperature, and heat exposure time; and to a lesser extent, pressure and nature of the environment. At maximum continuous service temperatures, thermal degradation of the resins is minimal. For example, at 400ƒC, FEP is measured at 4/100,000 of 1 percent, and PTFE at 1/100,000 of 1 percent. At high processing temperatures, adequate ventilation is recommended.

• High upper service temperature (260ƒC [500ƒF] for PTFE, 204ƒC [400ƒF] for FEP and 260ƒC [500ƒF] for PFA). The polymersí high melting points and morphological features allow components made from the resin to be used continuously at the stated temperatures. Above this temperature, the componentís physical properties may begin to decrease. The polymer itself, however, will be unaffected if the temperature is insufficient for thermal degradation.

• Insolubility–There is no known solvent for fluorocarbon resins under ordinary conditions.

• Inertness to chemical attack–The intrapolymer-chain bond strengths preclude reaction with most chemicals. Under relatively unusual circumstances the polymer can be made to react. Examples of unusual reagents include:
- Sodium, in a suitable media, etches the fluorocarbon polymer.
- Finely divided metals often interact with the polymer.
- Interhalogen compounds often induce halogen interchange with the fluorine.
- Ionized oxygen in oxygen plasma is often sufficiently energetic to react with the polymer chain.
- Electron bombardment at the megarad level can sever the polymer chain.

• Low coefficient of friction–The low coefficient of friction of results from low interfacial forces between its surface and another material and the comparatively low force to deform.

• Low dielectric constant and dissipation factor–provides low, if not the lowest, values for these parameters. These low values arise from the polymerís nonpolarity as well as the tight electron hold in the ultrapolymer bonds.

• Low water absorptivity–For to absorb water, the surface must remain wet for a long enough time for water to become physico-chemically associated with the polymer
chains, and then it must become included in the polymer bulk structure. Water is a very high energy material and has a very low surface energy. Therefore, these events are energetically incompatible and only occur under special circumstances and to a small extent.

• Excellent weatherability–Weather includes light of various wavelengths (IR, visible, UV), water (liquid or gas), other gases, and normal temperatures and pressure. The physical and chemical makeup of makes it inert to these influences.

• Flame resistant–will burn when exposed to flame, but will not continue to burn when the flame is removed.

• Excellent toughness–Some mechanical properties of resins are shown in Table 1. Toughness characteristics are high and differ somewhat between resin types.
© Copyright 2003-2012  |  OMEGA ENGINEERING, Inc. | OMEGA Privacy Statement  |  Terms and Conditions    MXV MMV | 72
HACKER SAFE certified sites prevent over 99.9% of hacker crime. VerisignAmex, Visa, Mastercard