Omega.com - Your one-stop source for process, measurement, and control Omega Engineering 1-888-TC-OMEGA(US & Canada) 1-203-359-1660 (International)
HomeQuick OrderProductsFree LiteratureMy OmegaOmega Info
View Cart Help Contact Us
Back to omega.com
RTDs
 
   What is a Resistance Temperature Detector (RTD)?



Product Links
View All RTDs
OEM Temperature Sensor Manufacturing
Quick Disconnect RTD Probes
General Purpose RTD Probes
Handle Probes
Industrial RTD Probes
RTD Elements with Lead Wires Attached
Wall Mount RTD Sensor
RTD Extension Cable
Extruder RTD Probes
PFA Coated Probes
Surface Measurement RTD Elements
Precision and Specialized RTD Probes
RTD Elements

Resistance Temperature Detectors / RTD / RTDs

What is a Resistance Temperature Detector? Resistance Temperature Detectors (RTD), as the name implies, are sensors used to measure temperature by correlating the resistance of the RTD element with temperature. Most RTD elements consist of a length of fine coiled wire wrapped around a ceramic or glass core. The element is usually quite fragile, so it is often placed inside a sheathed probe to protect it. The RTD element is made from a pure material whose resistance at various temperatures has been documented. The material has a predictable change in resistance as the temperature changes; it is this predictable change that is used to determine temperature.

Common Resistance Materials for RTDs:

  • Platinum (most popular and accurate)
  • Nickel
  • Copper
  • Balco (rare)
  • Tungsten (rare)
  •    An example of a Resistance Temperature Detector(RTD)


       Benefits of Using an RTD
    The RTD is one of the most accurate temperature sensors. Not only does it provide good accuracy, it also provides excellent stability and repeatability. Most OMEGA standard RTDs comply with DIN-IEC Class B. The accuracy of an OMEGA standard RTDs is shown in the table on the right.

    RTDs are also relatively immune to electrical noise and therefore well suited for temperature measurement in industrial environments, especially around motors, generators and other high voltage equipment.

    Accuracy for Standard OMEGA RTDs
    Temperature
    °C
      Ohms    °C  
    -200±056±1.3
    -100±0.32±0.8
    0±0.12±0.3
    100±0.30±0.8
    200±0.48±1.3
    300±0.64±1.8
    400±0.79±2.3
    500±0.93±2.8
    600±1.06±3.3
    650±1.13±3.6
    700±1.17±3.8
    800±1.28±4.3
    850±1.34±4.6


       Styles of RTDs
    RTD Elements
    The RTD element is the simplest form of RTD. It consists of a piece of wire wrapped around a ceramic or glass core. Because of their compact size, RTD elements are commonly used when space is very limited.
    1PT100G RTD Elements
    RTD Surface Elements
    A surface element is a special type of RTD element. It is designed to be as thin as possible thus providing good contact for temperature measurement of flat surfaces.
    "F" Series RTD Elements
    RTD Probes
    The RTD probe is the most rugged form of RTD. A probe consists of an RTD element mounted inside a metal tube, also known as a sheath. The sheath protects the element from the environment. OMEGA offers a wide variety of probes in various configurations.
    PR-10 RTD Probe
    RTD Terms
    » RTD (Resistance Temperature Detector)
    An acronym for resistance temperature detector or device. A resistance temperature detector operates on the principle of the change in electrical resistance in wire as a function of temperature.
    » RTD Element
    Sensing portion of the RTD which can be made most commonly of platinum, nickel, or copper. OMEGA features two styles of elements: wire wound and thin film.
    » RTD Probe
    An assembly composed of an element, a sheath, a lead wire, and a termination or connection. The standard OMEGA® RTD probe is made with a 100 ohm platinum European curve element (alpha = 0.00385).
    » Platinum RTD
    Also known as Pt RTD, Platinum RTD's are typically the most linear, stable, repeatable, and accurate of all RTD's. Platinum wire was chosen by OMEGA because it best meets the needs of precision thermometry.
    » Thin Film RTD
    Thinfilm RTD's are made up of of a thin layer of a base metal embedded into a ceramic substrate and trimmed to produce the desired resistance value. OMEGA RTD's are made by depositing platinum as a film on a substrate and then encapsulating both. This method allows for the production of small, fast response, accurate sensors. Thin film elements conform to the European curve/DIN 43760 standards and the “0.1% DIN” standard tolerance.
    » Class A RTD
    Highest RTD Element tolerance and accuracy, Class A (IEC-751), Alpha = 0.00385
    » Class B RTD
    Most Common RTD Element tolerance and accuracy, Class B (IEC-751), Alpha = 0.00385
    » Aplha .00385 Curve
    European Curve meets “0.1% DIN” standard tolerance and conforms to the DIN 43760 standard
    » Wire Wound
    The standard RTD elements used in OMEGA’s probe assemblies are made of 99.99% pure platinum wire wound about a ceramic or glass core and hermetically sealed within a ceramic or glass capsule.
    Automation |Accelerometers | Calibrators | Cartridge Heaters | Chart Recorders | Cryogenics | Custom Pressure Transducers | Data Loggers | Data Acquisition | Dial Thermometers | Fiber Optics | Flexible Heaters | Flowmeters | Glass Bulb Thermometers | Grippers | Heaters | Humidity Measurement | Immersion Heaters | Infrared Thermometers | Level Measurement | Load Cells | Magnetic Flow Meters | Panel Meters | Pressure Gauges | Pressure Transducers | Rotameters | RTD | Remote Process Monitoring | Signal Conditioners | Stepper Motors | Strain Gages | Strip Heaters | Temperature Controllers | Temperature Labels | Temperature Measurement | Temperature Sensor Manufacturing | Temperature Transmitters | Thermistors | Thermocouple | Thermocouple Wire | Thermowell | Ultrasonic Flow Meters