Accessibility  Skip navigation  Site Map  Help  Search field  View shopping cart  View shopping cart  Skip to Navigation
Omega.com - Your one-stop source for process, measurement, and control Omega Engineering 1-888-TC-OMEGA(US & Canada) 1-203-359-1660 (International)
Home Online Store Products Literature My Omega Omega Info Contact Us View Shopping Cart Help Global
Navigation Image Map   Help Icons image map
 
Order by part number
Product Manuals
Technical Reference
Calibration services
FTP Site
E-Quote
Product Handbook Index

Part Number Cross Reference


Click for Live, Online Support!!

Programming PCI Boards in DOS

The PCI bus offers simple "plug and play" capability to the end user in addition to other major advantages over the ISA bus. Users benefit because there are no switches or jumpers to be set in selecting the base address and interrupt required by a PCI data acquisition board like the PCI-DAS1602/16. The PCI BIOS makes these assignments when the system boots thereby guaranteeing that the your software can access the board. Contrast this with the ISA bus, where either a misplaced base address switch or a base address that conflicted with other hardware meant that one could not access the board in question.

How to determine the base address and interrupt of a PCI board

Since the base addresses of various registers in a board are set by the PCI BIOS, you will need to query the BIOS to determine these. This must be done before you access and/or program the board in any way. Before delving into the details we need to look at the PCI Configuration Header Space.

Each PCI bus device contains a unique 256-byte region called its configuration header space. The organization of this space is given in the table below. The important fields that are relevant to this discussion are named; the others are either reserved or not used.

31

23

15

7

 

Device ID

Vendor ID

00

         
         

Base address register #0

10

Base address register #1

14

Base address register #2

18

Base address register #3

1C

Base address register #4

20

         
     

Interrupt line

3C

The device and vendor IDs are unique values that are we assign to each PCI data acquisition board. These are used in querying the PCI BIOS for a specific board. The base address registers provide a mechanism for assigning I/O space. Registers in Omega. s family of PCI boards are offset from the I/O address contained in a specific base address register. For example, in the PCI-DAS1602/16 the ADC data can be read at the I/O address contained in base address register 2 and the DAC can be updated by writing to the I/O address contained in base address register 4.

The following code snippets describe the steps necessary to determine the contents of the various base address registers. The assembly language code is for Windows 3.1 or DOS. For the sake of clarity and brevity error handling code is not shown.

; ;PCI function values

PCI_FUNC_ID equ 0b1h

FIND_PCI_DEV equ 02h

READ_CONFIG_BYTE equ 08h

READ_CONFIG_WORD equ 09h

READ_CONFIG_DWORD equ 0ah

;Configuration register offsets

VID_ADDR equ 00h

DID_ADDR equ 02h

BADR0_ADDR equ 10h

BADR1_ADDR equ 14h

BADR2_ADDR equ 18h

BADR3_ADDR equ 1ch

BADR4_ADDR equ 20h

INTLN_ADDR equ 3ch

; Operation registers offsets

INTCSR_ADDR equ 38h

BMCSR_ADDR equ 3ch

;Misc. equates

IO_ADDR_MASK equ 0fffch

INTCSR_DWORD equ 00FF1F00H ; dword written to INTCSR_ADDR

BMCSR_DWORD equ 08000000H ; dword written to BMCSR_ADDR

;***************************************************************

; Macro to write a 32-bit dword to an I/O port. This is called

; from 16-bit code segment.

; Arguments : dwValue = DWORD value to write to port

; Uses : dx must have the port address

; Returns ; eax=dwValue

; Destroys : eax

;---------------------------------------------------------------

OUTD MACRO dwValue

db 66h ; OPSIZE:

db 0b8h ; mov eax

dd dwValue ; OPSIZE : mov eax, dwValue

db 66h, 0efh ; OPSIZE : out dx, eax

ENDM

;STEP 1 : Find the specific board.

mov dx, VENDOR_ID ; vendor id available from Omega Engineering Inc.

mov cx, PCI_DAS1602_DID ; device id available from Omega Engineering Inc.

mov si, 0

mov ah, PCI_FUNC_ID ;load pci function id into AH

mov al, FIND_PCI_DEV ;load search for device function into AL

int 1ah ;call bios ; Output: bl = device & function number

; bh = bus number

; CF set if error

;STEP 2 : Read the base address registers, using BX obtained earlier

mov di, BADR0_ADDR ;read base addr0

mov ah, PCI_FUNC_ID ;load PCI function id

mov al, READ_CONFIG_DWORD ;load read double word function

int 1ah ;call bios ; Output: ecx= register value, CF set on error

and cx, IO_ADDR_MASK

;At this point CX has the address contained in base address register 0. Repeat the above five instructions with the offsets of the other base address register in DI. You can store the contents of CX in some variable to avoid having to access the BIOS repeatedly.

; STEP 3 Find the interrupt used by the board.

mov di,INTLN_ADDR ;read the interrupt line reg

mov ah, PCI_FUNC_ID ;load PCI function id

mov al, READ_CONFIG_BYTE ;load read byte function

int 1ah ;bios interrupt call returns ch is zero, cl is IRQ#

;STEP 4 : Reset and enable interrupts if the board uses interrupts.

; First, copy base address 0 obtained earlier into DX

add dx, BMCSR_ADDR

OUTD BMCSR_DWORD ;reset mail box interrupts

sub dx, 4 ;dx=INTCSR_ADDR

OUTD INTCSR_DWORD ;reset pending interrupts and enable interrupts

The OUTD macro allows 32-bit I/O write to the Interrupt Control/Status register and Bus Master Control/Status Register.

© Copyright 2003-2009  |  OMEGA ENGINEERING, Inc. | OMEGA Privacy Statement  |  Terms and Conditions MXV MMV | 71
HACKER SAFE certified sites prevent over 99.9% of hacker crime. VerisignAmex, Visa, Mastercard