Chart Recorder for Temperature & Humidity

Volume discounts available
Volume Discount Schedule
Quantity | Price each |
---|---|
1-4 | $496.60 |
5-9 | $471.77 |
10-24 | $446.94 |
25-49 | $422.11 |
50-99 | $397.28 |
100+ | $372.45 |
Added to Your Shopping Cart
Configuration complete.
Please add to cart to keep it or exit the configuration
Please add to cart to keep it or exit the configuration
Failed to Save Configurations, Click on Configure Button Start Again
Chart Recorder for Temperature & Humidity is rated
out of
5 by
6.
- Charting Web Server Application
- Alarms by Email or Text Message
- Record Years of Data on Popular SD Cards
- Temperature
- Humidity
- Dewpoint
- No Special Software Required
- NEW Feature Added: Units with Dual Temperature and Humidity Probes
- Compatible with Omega Enterprise Gateway
- Download iServer Software
- Log data with Omega Enterprise Gateway(OEG)

Edit Options
View all modelsNot all combinations are valid. Options compatible with previous selections will be in bold.
*Highlighted options are not compatible. Please select a different combination.
Input Type
Input Ranges
Output Type
Display Type
Supply Voltage Type
Additional Feature
Product Specs
| ||
| ||
| ||
| ||
| ||
| ||
| ||
| ||
Rated 5 out of
5
by
Cjnngnr from
Great Features
We have incorporated this device in a Environmental Monitoring Unit for an Antenna Radome to provide us with historical data on the Environmental conditions within the Radome. We have storage data from one system for over 3 years recorded which allows feedback to the OEM of the Antenna and Radome.
Date published: 2017-01-31
Rated 1 out of
5
by
TTHT from
Device Does Not Connect and Bad Service
Ordered this device for alarms but it has difficulty connecting to network and randomly decides not to connect when hardwired to the computer for configuration. Omega has terrible customer service. Even with the warranty they did not help me fix my problem (took a year of me emailing and calling them before they responded). They sent me back the device saying there was no problem. It still does not work.
Date published: 2020-10-08
Rated 5 out of
5
by
meowcake from
Works as expected
Been installed in a proper machine shop with oil vapor and the likes.
Sensor element is trash in my opinion (5% change over 2 years) but designed to be replaced yearly if maintaining certification is your requirement. The iTHX device, although showing it's age, still trucks along just fine. Gathering data is easy and there is no software crippling (why I stay with Omega, it does what it says it does today and 10 years from now). Their documentation allows for anything from a highly engineered system's dev team to a script writer to easily integrate this sensor.
Exactly what was advertised, and has never had issues. Also, the last two sensors were of a higher caliber than previously. It's nice to be able to call someone at this price point as well.
Date published: 2016-09-27
Rated 1 out of
5
by
FrustratedITAdmin from
Solid devices with absolutely mediocre management
These devices run on ancient software, and forget their configured settings every time they lose power. They use 9V batteries for backup, which is not ideal because they can't be charged by the main power source, so if you need to deploy a bunch of these, it will be impossible to keep track of constantly replacing the batteries. The server product is difficult to find information on, and is also garbage with extremely limited features and functionality. They do not support WiFi or PoE for easy deployment options. The only pro to these is that they are accurate, and the device itself is very durable. Everything else stinkss though...look elsewhere.
Date published: 2021-01-11
Rated 5 out of
5
by
Booky from
Always performs to my expectations
I have been using these for years now and they keep on working.
Date published: 2018-02-15
Rated 5 out of
5
by
Ken1 from
Great service and products.
I bought this item and when I received it we found that it had a cracked probe. I called Omega and talked to an engineer about this and he immediately sent out a replacement with hardly no questions asked. It was also sent overnight at no charge to me. GREAT service and products.
Date published: 2017-06-01
According to the Product Spec sheet for Omega iTHX-SD Chart Recorders, regarding "Sensor and Calibration" it states "It is not necessary to take the iTHX-SD out of service for routine calibration." Does this mean that routine calibration is not required?
We sell the pre-calibrated probes, you could order them three or four weeks before the ones you have expire (that is typical lead time for you), that way you do not have to put your devices out of service.
Thank you.
Date published: 2019-07-18
Can I specify an SMTP server by hostname rather than IP address? This would be helpful since IP addresses are more likely to change than hostnames. Thank you.
I am sorry IP address is the only way to specify the SMTP server.
Date published: 2020-02-13
Received ours today Dec 23, 2019. Also am getting the HTProbe2 Error. Can an OMEGA engineer clear this up please?
Once you get the units connected on the network, you can change the setup on the IP page and the error will clear.
Date published: 2020-01-07
Hello I am unable to view the chart in win 10 pro or use the java selection. Ca you help
Due to security issues Java is no longer supported by web browsers there please click on the following link down load and install our Omega Enterprise Gateway software which you can use to monitor and log the data:
ftp://ftp.omega.com/public/DASGroup/products/OEG/Omega_Enterprise_Gateway_64bit.zip
Date published: 2020-02-12
I removed the SD card and saved the readings. When I re-install the card, the unit does not appear to be recording again. I have it wall-mounted and not connected to a computer or network. How do I get it to take readings again?
Please send your issues with ITHX-SD to DAS Tech Support -DAS@OMEGA.COM
Date published: 2020-05-28
Can the iTHX-SD be used as a handheld device to quickly take readings at multiple locations? Ultimately we plan to position the device in a permanent location and connect it to our network but I'm wondering if the device can also be used as a handheld.
Hello I am sorry it is not designed as a hand held device you cannot start and stop the device except using a PC through the network to send commands.
Date published: 2019-11-21
How do you use the alarm relay function on the iTHX-SD to drive a stacklight visual alarm or audible buzzer alarm? What equipment would be required to do this?
Please e-mail your question to Das Engr Dept-DAS@OMEGA.COM and they will try to assist you.
Date published: 2020-12-16
DISCONTINUED - iServer MicroServerâ„¢ Barometric Pressure, Temperature, and Humidity Transmitters
$17.22
0 In Stock
iServer MicroServerâ„¢ Barometric Pressure, Temperature, and Humidity Transmitters
$24.28
0 In Stock