Skip to search Skip to main content Skip to navigation

Call us at 1-888-826-6342

We noticed you are from . Visit your local site for regional offers and live support.


800 Connecticut Ave., Norwalk CT 06854

Certificate of Compliance
for Directive 2011/65/EC of the European Parliament and of the Council of 8 June 2011 on the restriction of use of certain hazardous substances in electrical and electronic equipment.

The directive 2011/65/EC defines six (6) substances which are to be restricted. The maximum concentration by weight for each substance is listed below.

Substance Maximum Concentration 1
Lead (Pb) 0.1%2
Mercury (Hg) 0.1%
Cadmium (Cd) 0.01%
Hexavalent Chromium (Cr VI) 0.1%
Polybrominated biphenyls (PBB) 0.1%
Polybrominated diphenyl ethers (PBDE) 0.1%

1 Restricted substances and maximum concentration values tolerated by weight in homogeneous materials

2 Exemption 6(a) Lead as an alloying element in steel for machining purposes and in galvanized steel containing up to 0.35 % lead by weight; Exemption 6(b) Lead as an alloying element in aluminum containing up to 0.4 % lead by weight; Exemption 6(c) Copper alloy containing up to 4 % lead by weight; and Exemption 7(c)-I Electrical and electronic components containing lead in a glass or ceramic other than dielectric ceramic in capacitors, e.g. piezoelectronic devices, or in a glass or ceramic matrix compound.

Part Number: RLC-80-0-100-10

RoHS2 Status: Compliant

Based upon a review of the manufacturing records and technical information, this product, to the best of our knowledge, does not contain any of the restricted substances in quantities that exceed the limits, as specified above.

If you have a question in regards to the RoHS status of this product please contact the Product Compliance Group.
04/16/2024

Omega Engineering Inc.
Global Product Compliance Group

en-US
en
Save Configuration