Call us at 1-888-826-6342
Call us at 1-888-826-6342
Certificate of Compliance
for EU Directive 2011/65/EU and 2015/863 of the European Parliament on the restriction of use of certain hazardous substances in electrical and electronic equipment.
The directive 2015/863 defines ten (10) substances which are to be restricted. The maximum concentration by weight for each substance is listed below.
Substance | Maximum Concentration 1 |
---|---|
Lead (Pb) | 0.1%2 |
Mercury (Hg) | 0.1% |
Cadmium (Cd) | 0.01% |
Hexavalent Chromium (Cr VI) | 0.1% |
Polybrominated biphenyls (PBB) | 0.1% |
Polybrominated diphenyl ethers (PBDE) | 0.1% |
Bis(2-ethylhexyl) phthalate (DEHP) | 0.1% |
Butyl benzyl phthalate (BBP) | 0.1% |
Dibutyl phthalate (DBP) | 0.1% |
Diisobutyl phthalate (DIBP) | 0.1% |
1 Restricted substances and maximum concentration values tolerated by
weight in homogeneous materials
2 Exemption 6(a) Lead as an alloying element in steel for machining purposes and in galvanized
steel containing up to 0.35 % lead by weight; Exemption 6(b) Lead as
an alloying element in aluminum containing up to 0.4 % lead by
weight; Exemption 6(c) Copper alloy containing up to 4 % lead by
weight; and Exemption 7(c)-I Electrical and electronic components
containing lead in a glass or ceramic other than dielectric ceramic
in capacitors, e.g. piezoelectronic devices, or in a glass or ceramic
matrix compound.
Part Number: TJ36-CAXL-020G-12-SMPW-M
RoHS 2015/863 Status: Compliant
Based upon a review of the manufacturing records and technical information, this product, to the best of our knowledge, does not contain any of the restricted substances in quantities that exceed the limits, as specified above.
If you have a question in regards to the RoHS status of this product please contact the Product Compliance Group.
04/25/2024
Omega Engineering Inc.
Global Product Compliance Group