Skip to search Skip to main content Skip to navigation

Call us at 1-888-826-6342

We noticed you are from . Visit your local site for regional offers and live support.
Blog Stop! Calibrate and Listen

Stop! Calibrate and Listen Calibration is crucial in industrial manufacturing because it ensures the accuracy and reliability of measurement instruments and equipment used in production processes. With proper calibration, manufacturing professionals can verify performance against recognized standards and initiate adjustments, if necessary.

Read More
Blog Tapping the Keg of Innovation - Omega's Unparalleled Temperature Measurement Technology is the Craft Brewer's Newest Secret Ingredient

Tapping the Keg of Innovation - Omega's Unparalleled Temperature Measurement Technology is the Craft Brewer's Newest Secret Ingredient Innovation is, and always has been, the fuel that drives the Craft Beer Brewing Industry – from fostering creativity to propelling industry dynamics, it is a main contributor to both growth and evolution.

Read More
Blog Enabling On-Shoring of Critical Water/Wastewater Infrastructure with Omega’s New <br>Non-Invasive Temperature Sensor for Plastic Pipes

Enabling On-Shoring of Critical Water/Wastewater Infrastructure with Omega’s New
Non-Invasive Temperature Sensor for Plastic Pipes
After years of ongoing challenges with the global supply chain, ResinTech Inc, a resin manufacturer and global leader in ion exchange for water purification, built the first new ion exchange factory in the US in more than 30 years.  Inside, ResinTech manufactures its own high quality ion exchange resin from scratch to rigid specifications.

Read More
Blog A Need for Speed: How Omega’s Innovative Temperature Sensing Technology was used to Expedite the Commission of a Productivity Enhancing Investment

A Need for Speed: How Omega’s Innovative Temperature Sensing Technology was used to Expedite the Commission of a Productivity Enhancing Investment The brewing team at Allagash Brewing Company successfully utilized the versatility, non-invasiveness, and high accuracy of the HANI Clamp Temperature Sensor – which clamps right onto the outside of a desired pipe and measures the fluid inside with as much accuracy and with the same high performance as traditional sensors – to expedite the commissioning process and meet their ROI of an important investment to their system.

Read More
Blog HANI Temperature Sensor Chosen as Finalist in Best of Sensors Awards

HANI Temperature Sensor Chosen as Finalist in Best of Sensors Awards Sensors Converge is almost here! Sensors Converge began as a show focused solely on sensor technology, and has evolved over the years to a large event focusing on not only sensors, but also the complex systems that work with them. The 2023 show will be held June 20-22 in Santa Clara, CA at the Santa Clara Convention Center.

Read More
Blog A Need for Speed: How HANI Technology Was Used to Expedite the Commission of a Productivity Enhancing Investment

A Need for Speed: How HANI Technology Was Used to Expedite the Commission of a Productivity Enhancing Investment The brewing team at Allagash Brewing Company successfully utilized the versatility, non-invasiveness, and high accuracy of the HANI Clamp Temperature Sensor – which clamps right onto the outside of a desired pipe and measures the fluid inside with as much accuracy and with the same high performance as traditional sensors – to expedite the commissioning process and meet their ROI of an important investment to their system.

Read More
Blog The Future is Bright: Omega’s Own Co-Op Wins Prestigious Award

The Future is Bright: Omega’s Own Co-Op Wins Prestigious Award The Omega Co-Op/Internship Program was created to help students grow and realize their full potential - setting them up with the experiences and tools needed to excel in their future careers. We sit down with one of our latest engineer co-ops, David Austin, to find out more about his time with Omega and his recent award from Drexel University.

Read More
Blog Balls Out

Balls Out Have you ever heard someone use the term ‘balls out’? You know, as in giving it maximum effort or going all out. Have you ever wondered where the term comes from? Well, the truth is it probably doesn’t mean what you think it does. For the origins of the term, we need to go back to the late eighteenth century, when Scottish inventor and mechanical engineer James Watt was looking for a way to automatically regulate the speed of a steam engine.

Read More
Blog HANI: The Shortcut that ACTUALLY Works

HANI: The Shortcut that ACTUALLY Works Getting the accurate temperature of media flowing through a pipe is a serious pain in the neck. And, up until now, there really has only been one viable option: immersion sensors. But now there is another option: the HANI. It's quick, it's accurate, its non-contact. The HANI temperature sensor is the short cut that actually works.

Read More
Blog Measuring Temperature of Media Flowing Through a Pipe

Measuring Temperature of Media Flowing Through a Pipe The first way you might attempt to measure the temperature of a fluid moving through a pipe or inside a tank is to use a surface sensor.

Read More
Technical Learning How to Monitor Walk-In Freezer Temperatures with IIoT Devices

How to Monitor Walk-In Freezer Temperatures with IIoT Devices Maintaining optimal freezer temperatures is essential in protecting quality, ensuring food safety & reducing waste. Learn how companies are using Omega's products.

Read More
Technical Learning An Introduction to Industrial pH Measurement and Control

An Introduction to Industrial pH Measurement and Control In this article how pH describes the degree of acidity or alkalinity of a solution and how is measured is explained. Click here to learn how it´s done.

Read More
Technical Learning Types of Accelerometers

Types of Accelerometers An accelerometer is a device that can measure acceleration experienced by an object. However, there are many types of accelerometers. In this article you will learn about those.

Read More
Technical Learning What to Look for When Selecting Accelerometers?

What to Look for When Selecting Accelerometers? There are some specifications that you should always look when selecting an accelerometer. In this article the most important factors are explained.

Read More
Technical Learning What is a Calibration Certificate?

What is a Calibration Certificate? Calibration certificates validate the device’s accuracy levels to a standardized reference.

Read More
Technical Learning How to Use a Magnetic Flow Meter to Meet Hygiene Requirements for Clean-in-Place (CIP) Systems

How to Use a Magnetic Flow Meter to Meet Hygiene Requirements for Clean-in-Place (CIP) Systems In the food and beverage industry, clean-in-place (CIP) maintenance is essential for meeting safety and hygiene standards while maintaining process efficiency and maximizing equipment service life.

Read More
Technical Learning Measurement of Outflow Facility in the Eye

Measurement of Outflow Facility in the Eye Glaucoma is a world-leading cause of blindness. The major risk factor for glaucoma is elevated intraocular pressure (IOP), with the sole treatment for glaucoma patients being to reduce the IOP.

Read More
Technical Learning Best Practices: 3 Steps to Efficiency and Flexibility for Small Businesses using IIoT

Best Practices: 3 Steps to Efficiency and Flexibility for Small Businesses using IIoT Operational efficiency is key to the success of any small business, and IIoT essentially helps you achieve that by turning your offline processes to online through a connected environment.

Read More
Hub

RTD sensors Introduction to Pt100 RTD Temperature Sensors

Read More
Hub

IIOT - Industrial Internet of Things IIoT or Industrial Internet of Things is one such technology that is mostly unknown to non-extert. In this article, IIoT is explained in detail.

Read More
Technical Learning How Do Infrared Thermometers Work?

How Do Infrared Thermometers Work? Infrared (IR) forehead thermometers are useful in measuring temperature across a range of industrial and clinical environments.

Read More
Technical Learning Infrared Thermometers: FAQs

Infrared Thermometers: FAQs It is essential to understand that the accuracy of IR thermometers depends on how and where you use them.

Read More
Technical Learning Most common applications of Infrared Thermometers

Most common applications of Infrared Thermometers Because of their ability to measure temperature from a distance, IR thermometers have a broader scope of application than just checking whether you have a fever.

Read More
Technical Learning 7 Key Benefits of Remote Monitoring Using IIoT

7 Key Benefits of Remote Monitoring Using IIoT Businesses can overcome challenges by leveraging the IIoT-enabled remote monitoring framework and achieve substantial improvements.

Read More
Technical Learning Give Your Legacy Systems an IIoT Upgrade and Achieve More

Give Your Legacy Systems an IIoT Upgrade and Achieve More The most common obstacle is collecting operational data from legacy machines and communicating that data to the cloud.

Read More
Technical Learning Advantages of New OMEGA PCC-SMD for Cold Junction Compensation

Advantages of New OMEGA PCC-SMD for Cold Junction Compensation OMEGA’s new PCC-SMD unique features make integration of cold junction compensation easier than it ever has been before.

Read More
Technical Learning Best Practices to Implement Temperature Screening

Best Practices to Implement Temperature Screening As businesses plan to resume operations with the easing lockdown restrictions, the immediate challenge for them is to keep their employees and customers safe.

Read More
Technical Learning Real-World Examples of IIoT Monitoring

Real-World Examples of IIoT Monitoring Here, we explore two typical use cases and corresponding real-world examples of IIoT monitoring solutions.

Read More
Technical Learning How to Trigger an Alarm When Freezer Door Is Left Open

How to Trigger an Alarm When Freezer Door Is Left Open When a freezer door is accidentally left partially open, it can lead to food spoilage and increased energy costs.

Read More
Technical Learning How to Monitor Asphalt Temperature with IIoT Devices

How to Monitor Asphalt Temperature with IIoT Devices The temperature of hot mixed asphalt is a critical component to the compaction and longevity of poured concrete.

Read More
Technical Learning How to Connect Your Modbus Devices to the Omega Link Gateway

How to Connect Your Modbus Devices to the Omega Link Gateway Industrial setups look to reap the benefits of the Industrial Internet of Things (IIoT) by establishing a connected environment.

Read More
Product Info Remote monitoring for challenging times

Remote monitoring for challenging times How can remote monitoring help your application stay afloat and keep employees safe

Read More
Technical Learning 5 Ways Smart Sensor Data Brings Benefits for Your Business

5 Ways Smart Sensor Data Brings Benefits for Your Business Smart technology is expanding its horizons to sensor products, and it has completely changed the concept, integration, and application of these devices.

Read More
Technical Learning What is Edge Computing?

What is Edge Computing? The concept of edge computing has been around for several years, stemming from the days of on-premise Computer Instrumentation or Human Machine Interface (HMI) computers.

Read More
Product Info What are Load Cells and How Do They Work?

What are Load Cells and How Do They Work? A load cell is a transducer which converts force into a measurable electrical output.

Read More
Technical Learning How to select Heat Trace Cable?

How to select Heat Trace Cable? Selecting the proper cable family according to the process conditions is necessary to get desired temperature controls within the pipes.

Read More
Technical Learning What is a Heat Trace System?

What is a Heat Trace System? A heat trace system is a set of paths lined along pipes or vessels.

Read More
Technical Learning Designing the Right Heat Trace System

Designing the Right Heat Trace System Designing a perfect heat trace system requires considering several important variables.

Read More
Technical Learning What is a type K Thermocouple?

What is a type K Thermocouple? A Type K thermocouple refers to any temperature sensor containing Chromel and Alumel conductors, that meets the output requirements as stated in ANSI/ASTM E230 or IEC 60584 for Type K thermocouples

Read More
Technical Learning What Are The Most Common Applications for Thermocouples?

What Are The Most Common Applications for Thermocouples? Thermocouples are used in a wide range of applications.

Read More
Technical Learning How to Mount Thermocouples Correctly?

How to Mount Thermocouples Correctly? When connecting thermocouples to other devices care needs to be taken to ensure that the proper polarity is maintained.

Read More
Technical Learning FAQ: Thermocouple Characteristics and Specifications

FAQ: Thermocouple Characteristics and Specifications Thermocouples do have positive and negative wires, in order to read a correct temperature the polarity needs to be maintained throughout the circuit.

Read More
Technical Learning Thermocouple Styles and Constructions

Thermocouple Styles and Constructions Thermocouples come in three types of junctions, Grounded, Ungrounded and Exposed.

Read More
Technical Learning Common Techniques to Calibrate Thermocouples

Common Techniques to Calibrate Thermocouples Thermocouples are usually calibrated in one of three ways depending on the accuracy needed and the conditions where the calibration takes place.

Read More
Technical Learning FAQ: Thermocouple Installations

FAQ: Thermocouple Installations When more than one measurement is needed, dual thermocouples provide that extra measurement signal.

Read More
Technical Learning Pressure Transducer in Underwater Applications

Pressure Transducer in Underwater Applications A pressure transducer being underwater presents its own unique challenges.

Read More
Technical Learning Pressure Transducer and Controllers

Pressure Transducer and Controllers Pressure not only needs to be measured, but your system needs to make changes based on pressure readings as well.

Read More
Technical Learning Pressure Transducer and Amplifier Selection

Pressure Transducer and Amplifier Selection Choosing the proper amplifier depends on the type of signal that your system needs.

Read More
Technical Learning Pressure Transducer for Gases

Pressure Transducer for Gases ‘Gas’ is an incredibly broad term. Many industries use gas, but not every industry needs to accurately measure the pressure of the system.

Read More
Technical Learning Pressure Transducer for Air

Pressure Transducer for Air Air pressure was first measured all the way back in 1643: when the barometer was invented.

Read More
Technical Learning Pressure Transducer in Air Applications

Pressure Transducer in Air Applications There are a wide variety of applications that need air pressure properly monitored.

Read More
Technical Learning Pressure Transducers and Dataloggers

Pressure Transducers and Dataloggers Data loggers are typically used to measure and store the pressure signals that a system puts out.

Read More
Technical Learning Choosing a Signal Transmitter

Choosing a Signal Transmitter From reviewing both devices and the way they work with other devices, it is clear that signal transmitters and signal conditioners more or less perform the same set of tasks.

Read More
Technical Learning Signal Transmitters

Signal Transmitters A signal transmitter is a device that transmits data from one place to another.

Read More
Technical Learning Why IoT Isn’t Good Enough for Industrial Applications

Why IoT Isn’t Good Enough for Industrial Applications Whenever there's a discussion about IIoT, a comparison with IoT always exists.

Read More
Technical Learning What components are in a IIoT network?

What components are in a IIoT network? IIoT or Industrial Internet of Things is one such technology that is well-known among industry experts but mostly unknown to the rest.

Read More
Technical Learning Pressure Measurement of Water Level

Pressure Measurement of Water Level Figuring out how much the water level has risen or fallen in a tank (or something similar) should be a simple task.

Read More
Technical Learning Pressure Transducers for Refrigerant

Pressure Transducers for Refrigerant Plenty of systems in the real world rely on the refrigeration cycle; from massive supermarket refrigeration systems to the AC unit in your car.

Read More
Technical Learning Pressure Transducer Specs

Pressure Transducer Specs Pressure transducers are useful in a variety of industries.

Read More
Technical Learning Pressure Transducer FAQ

Pressure Transducer FAQ Pressure sensors may undergo contamination from the environment around it or from the working fluid that it measures.

Read More
Technical Learning Testing Pressure Transducers

Testing Pressure Transducers Pressure transducers are precise instruments, and like all instruments, they are prone to failure.

Read More
Technical Learning Pressure Calibration Procedure

Pressure Calibration Procedure Calibration is an important step that helps devices to produce accurate measurements.

Read More
Technical Learning Which type of infrared sensing technology will work better for my application—an infrared thermometer or a thermal imaging camera?

Which type of infrared sensing technology will work better for my application—an infrared thermometer or a thermal imaging camera? There are many applications that require accurate surface temperature measurement but don’t permit the use of a surface probe because it’s not possible to make direct contact with the object whose temperature is being measured.

Read More
Technical Learning How do you split a thermocouple signal?

How do you split a thermocouple signal? Thermocouples are simple, low-cost, thermoelectric temperature sensors. They’re used in a wide range of temperature measurement processes and applications.

Read More
Technical Learning How to calculate heater wattage to get to the right temperature?

How to calculate heater wattage to get to the right temperature? When selecting a surface heater for use in an industrial process or application, you’ll want to begin by calculating your wattage requirements.

Read More
Technical Learning How to use a pressure transmitter or pressure transducer to measure the height of a column of water in a container?

How to use a pressure transmitter or pressure transducer to measure the height of a column of water in a container? Outlining the setup of an experimental application in which we use a pressure transmitter to measure the amount of pressure that’s being exerted by a column of water in a water bottle.

Read More
Technical Learning Why is it so difficult to calibrate a surface probe?

Why is it so difficult to calibrate a surface probe? Surface probes house may types of temperature measurement assemblies, including widely-used thermocouples.

Read More
Technical Learning Types of Signal Conditioners

Types of Signal Conditioners Signal conditioners are devices that modify output signals produced by a sensor.

Read More
Technical Learning How to use Load Cells for Weight Measurement

How to use Load Cells for Weight Measurement To measure the weight, the subject is placed on a load application point of a load cell.

Read More
Technical Learning Load Cell Specifications

Load Cell Specifications In this article all the specifications in a load cell's datasheet are explained. Click here to learn and understand more about the technical aspects.

Read More
Technical Learning How to Test a Load Cell?

How to Test a Load Cell? Set the multimeter in millivolts and connect the output wires of the load cell to it. Supply a excitation voltage and place a test weight on the load cell.

Read More
Technical Learning Why Load Cell Signal Conditioner is Critical to a Strain Gauge Setup

Why Load Cell Signal Conditioner is Critical to a Strain Gauge Setup Signal conditioners take the output from the load cell, modify it and then send it to digital monitors or data loggers.

Read More
Technical Learning How to Pick a Data Logger for Your Load Cell?

How to Pick a Data Logger for Your Load Cell? A force to a load cell causes deformation on the strain gauge creating a electrical signal. A data logger takes that data and stores the data for later.

Read More
Technical Learning Load Cell Meter: Choosing the Right Strain Meters

Load Cell Meter: Choosing the Right Strain Meters The load cell meter connects directly to the strain gauge to convert the signal into a displayed value. They can also power up the load cell.

Read More
Technical Learning Load Cell FAQ

Load Cell FAQ Have questions about load cells?

Read More
Technical Learning Load Cell with Remote Display

Load Cell with Remote Display To accurately read and process the load cell values, displays form an essential part of the weighing system.

Read More
Technical Learning Load Cell Controller

Load Cell Controller A load cell controller is a device used in conjunction with a load cell to convert the electrical signals from the load cell to readable real-world values.

Read More
Technical Learning Load Cell Platform Scale – Example Illustration

Load Cell Platform Scale – Example Illustration For high-precision weighing applications, load cell platform scales must measure the load accurately. To illustrate this measurement precision, an example with a test weight is explained here.

Read More
Technical Learning What is a Load Cell Amplifier?

What is a Load Cell Amplifier? A load cell amplifier is a device that can increase the strength of signals coming from a load cell.

Read More
Technical Learning USB Load Cells: Do More with the Measurement Data

USB Load Cells: Do More with the Measurement Data Analog load cells can't record the data for further analysis. To make the load cell signals readable by a computer an USB output is useful. Read it here.

Read More
Technical Learning An Introduction to 3-A Sensors for Sanitary Applications

An Introduction to 3-A Sensors for Sanitary Applications 3-A standards were developed in the 1920’s as way to qualify processes as being sanitary. The objective is to prevent contamination of products produced for human consumption or direct contact.

Read More
Application

How to Locate a Water Leak Using an Ultrasonic Flow Meter When a single conduit line in a complex configuration of pipelines is compromised, it can be challenging to locate the precise point where the leak is occurring.

Read More
Application

How to Measure an Industrial Coffee Grinder Motor’s Temperature During Grinding In this application, the purpose is to measure the temperature of the motor in an industrial coffee grinder during the grinding process to better understand the strain on the motor.

Read More
Application

How to Wirelessly Monitor Temperature for Performance Testing As part of the quality assurance process on refrigeration equipment such as refrigerators, freezers, and cold rails, there is a need to validate that the equipment is operating within specified parameters.

Read More
Application

Benchtop Controller for Mantle Heater Heating mantles are commonly used in laboratories to heat liquids as part of the research process.

Read More
Application

How to Achieve Precise Temperature Regulation of Experimental Materials Using a PID-Controlled Heat Source in Laboratory Applications To investigate whether the thermochromic phase change behavior of polydiacetylene thin films will be altered when placed onto a carbon substrate such as graphene, a researcher developed a transfer heat block whose temperature could be regulated over time.

Read More
Application

How to Monitor pH Levels in a High-Temperature Environment In a process application, such as soaking wood in a water bath, unpleasant odors can be omitted. By neutralizing pH levels in the water bath, odors can be controlled.

Read More
Application

How to Measure pH Levels in a Ruminant’s Digestive System The pH levels in each of a ruminant’s four stomachs play an essential role in a cow’s digestive process and milk production.

Read More
Application

How to Dynamically Measure Load and Vibration in Final Product Testing for Bicycle Manufacturing As part of a quality assurance process, a bike manufacturer developed a testing system that could quantify load and vibration forces on the physical parameters.

Read More
Application

How to Test Load Tolerance in Control Cable Product Testing Control cables play a critical role in assuring the safety and operational integrity of a wide variety of mechanical and electromechanical devices, including lawn mowers and bicycles.

Read More
Application

Measuring the Force Applied to a Rocket Parachute Rockets deploy parachutes to aid in rapidly decreasing the rocket’s re-entry or landing speed. However, before use, it’s essential to test the system using s-beam load cells.

Read More
Application

How to Measure the Bending Force of a Sheet Metal Bending Machine Measuring bending stress requires determining the average amount of force exerted on the material that results in a repeatable uniform surface.

Read More
Application

How to Determine the Force Measurement of a Crossbow Crossbows work like a spring. The force and tension applied as you pull the string of the crossbow is what creates the movement and energy to propel the arrow from the bow at high speed.

Read More
Application

Flow of Paper Stock A customer in the paper industry wanted to measure flow of paper stock pulp on a 250mm SS line with an average flow of 120-150 l/s and a pulp temperature of 45°.

Read More
Application

Sanitary Precision Flow Measurement for Microbreweries All microbreweries need the ability to measure the liquid flow of their product in a manner that is sanitary and meets FDA regulations.

Read More
Application

How to Bend Guitar Sides with a Silicone Heater There are several ways to bend guitar sides, including the traditional method of using a hot pipe. However, a faster and more cost-efficient method, which has become common, involves using flexible silicone heaters with a flexible thermocouple and controller.

Read More
Product Info Thermal Imaging Camera

Thermal Imaging Camera A thermal imager is a non-contact temperature measurement device.

Read More
Technical Learning How thermal cameras are used in Home Inspections?

How thermal cameras are used in Home Inspections? Thermographic inspections uncover a wide variety of information to help you derive crucial details about your home. Learn more about this application here.

Read More
Technical Learning Top Applications of Thermal Imaging Cameras

Top Applications of Thermal Imaging Cameras In this article some of the most common applications of thermal imagers in a varied set of industries. Click here to discover those.

Read More
Technical Learning How to choose a Thermal Camera?

How to choose a Thermal Camera? Apart from cost and quality, the two major factors that you should keep in mind when buying a thermal imager are Detector Resolution and Thermal Sensitivity.

Read More
Technical Learning FAQ about Thermal Cameras

FAQ about Thermal Cameras Choosing a thermal imaging camera is tricky as they are different from other imaging technologies. Click here to learn about the questions that always puzzle buyers.

Read More
Technical Learning Water Hammer

Water Hammer Water hammer effect is an impact load that is the most misunderstood force known to pressure transducers today. A water hammer is created by stopping and/or starting a liquid flow suddenly.

Read More
Technical Learning Conductivity and Resistivity

Conductivity and Resistivity Conductivity measures the ability of a solution to conduct an electric current between two electrodes. In solution, the current flows by ion transport.

Read More
Product Info An Introduction to Flow Meters

An Introduction to Flow Meters As the name implies a Flow meter is an instrument for monitoring, measuring, or recording the rate of flow, pressure, or discharge of liquids or gasses.

Read More
Technical Learning How Does a Pressure Transducer Work?

How Does a Pressure Transducer Work? A pressure transducer is a device that measures the pressure of a fluid, indicating the force the fluid is exerting on surfaces in contact with it.

Read More
Technical Learning 4-20mA Input

4-20mA Input It is extremely simple and inexpensive to measure 4-20ma signal with a device that will measure only Voltage inputs.

Read More
Technical Learning Digital Signal Transmission

Digital Signal Transmission Industrial networks that transmit data using digital signals often are an integral part of a data acquisition or process control solution.

Read More
Technical Learning Digital Signal Transmission

Digital Signal Transmission In contrast to analog transducers that sense continuous variables such as pressure and temperature, many transducers provide an output that is one of two states: high or low, open or closed.

Read More
Technical Learning Everything you need to know about Immersion Heaters

Everything you need to know about Immersion Heaters An immersion heater is a device which is installed in a tank or container to heat a liquid. The installation can be over-the-side, flanged, or threaded.

Read More
Technical Learning What is a Polyimide Heater?

What is a Polyimide Heater? Polyimide heaters, also known as Kapton heaters, are made from Kapton, a polyimide film developed by DuPont.

Read More
Technical Learning Tape and Rope Heaters

Tape and Rope Heaters Rope and tape heaters are flexible heaters designed to wrap around pipes, beakers, and other round surfaces. Rope and tape heaters are very similar in that they have similar power densities and construction.

Read More
Technical Learning What are silicone heaters used for?

What are silicone heaters used for? Silicone rubber heaters have a wide range of industrial, commercial, and military applications. These heaters are resistant to radiation, moisture, compression set, weathering, vacuum, fungus, oils, solvents, and chemical attack.

Read More
Technical Learning Sales Measures Water Levels

Sales Measures Water Levels Customer service that goes above and beyond in combination with excellent products at competitive prices.

Read More
Technical Learning Safe and Precise Temperature Transmission and Control

Safe and Precise Temperature Transmission and Control Stable, safe, and high precision measurement of temperature signals in all stages of the manufacturing process is of the essence at a polysulfide plant.

Read More
Technical Learning Quality, Support, and Flexibility

Quality, Support, and Flexibility When it was time to exchange an old panel that controlled a hydrogen compressor an automation technician decided to go with a backplane.

Read More
Technical Learning Problem Solver in the Field

Problem Solver in the Field A project of operating a brand new waste-to-energy line gave an electrical engineer the chance to work with a field mounted HART temperature transmitter like TXUN-HT for the first time.

Read More
Technical Learning With an Isolated Repeater/Splitter

With an Isolated Repeater/Splitter A provider of electrical solutions to a wide range of customers and other electrical contractors, from temperature and pressure measurements to providing small PLC solutions needed a solution when working with temperature and isolation.

Read More
Technical Learning Danish CHP Station

Danish CHP Station The members of a maintenance team at a Danish power station were fed up getting error messages and false system alarms from one of the boiler’s temperature surveillance systems.

Read More
Technical Learning What is a Mass Flow Meter?

What is a Mass Flow Meter? A thermal mass flow meter measures the flow rate of gas mass based on the convective heat transfer of a heated surface to the flowing fluid.

Read More
Technical Learning What is a Coriolis Flow Meter and How Does it Work?

What is a Coriolis Flow Meter and How Does it Work? A Coriolis flow meter is a type of mass flow meter. It is designed differently and works differently than thermal or differential mass flow meters.

Read More
Case Study The International Temperature Scale of 1990 (ITS-90)

The International Temperature Scale of 1990 (ITS-90) President of the Comité Consultatif de Thermométrie and Vice-President of the Comité International des Poids et Mesures Division of Physics, National Research Council of Canada, Ottawa, K1A OS1 Canada

Read More
Technical Learning Thermocouple vs RTDs

Thermocouple vs RTDs Selecting the best temperature sensor for your application can be a challenge. A broad range of sensors are available today, and the better you understand the key differences between them

Read More
Technical Learning Principles of Infrared Thermocouples

Principles of Infrared Thermocouples The IRt/c product line represents a dramatic breakthrough in temperature sensing technology. The IRt/c sensors are unpowered, low cost, and can measure surface temperatures of materials without touching.

Read More
Product Info Thermocouple styles: probe, wire or surface?

Thermocouple styles: probe, wire or surface? Because a thermocouple can take many shapes and forms, it is important to understand how to correctly select the right sensor.

Read More
Technical Learning What is a Vortex Flow Meter?

What is a Vortex Flow Meter? A vortex flow meter is a flow measurement device best suited for flow measurements where the introduction of moving parts presents problems.

Read More
Technical Learning Thermocouple types

Thermocouple types Thermocouples are available in different combinations of metals or calibrations. The most common are the “Base Metal” thermocouples known as Types J, K, T, E and N.

Read More
Product Info What is a PID Controller?

What is a PID Controller? A PID controller is an instrument used in industrial control applications to regulate temperature, flow, pressure, speed and other process variables.

Read More
Technical Learning Thermocouple Response Time

Thermocouple Response Time Time constants calculated for air at room temperature and atmospheric pressure moving with velocity of 65 feet per second for thermocouples

Read More
Case Study Connecting Relays to a Digital Output Board and Noise Considerations

Connecting Relays to a Digital Output Board and Noise Considerations Mechanical relays are very noisy (electrically) and they can cause problems when connecting them to a PC digital I/O card, ranging from spikes on your analog measurements to computer lockups!

Read More
Technical Learning Thermocouples - Reference Guide

Thermocouples - Reference Guide OMEGACLAD® is a three-part system composed of compacted MgO insulation, thermocouple wire and metal sheath.

Read More
Product Info How to choose a Thermocouple

How to choose a Thermocouple There are different types of thermocouples and their applications may vary. An exposed thermocouple will work best when high response times are required, but an ungrounded thermocouple is better in corrosive environments

Read More
Product Info How to Choose Between a RTD PT100 vs Pt1000?

How to Choose Between a RTD PT100 vs Pt1000? The sensing elements in Resistance Temperature Detectors (RTD’s) can be categorized in terms of the type of metal out of which they’re made and their resistance at a benchmark temperature.

Read More
Product Info Types of RTDs

Types of RTDs Resistance Temperature Detectors (RTDs) available today can generally be categorized into one of two basic types of RTDs, depending on how their temperature sensing element is constructed.

Read More
Product Info What Are the Differences Between 2-Wire, 3-Wire, and 4-Wire RTD Configurations?

What Are the Differences Between 2-Wire, 3-Wire, and 4-Wire RTD Configurations? A Resistance Temperature Detector (RTD) measures temperature using a resistor with a resistance value that changes as its temperature increases or decreases.

Read More
Technical Learning Practical Guidelines for Temperature Measurement

Practical Guidelines for Temperature Measurement Temperature can be measured via a diverse array of sensors. All of them infer temperature by sensing some change in a physical characteristic.

Read More
Technical Learning Pt100 Probes

Pt100 Probes Probes may be terminated in a connection head, quick disconnect, terminal block, or extension wire. OMEGA’s standard terminations are pictured on product pages.

Read More
Technical Learning Resistance Elements and RTD’s

Resistance Elements and RTD’s Resistance elements come in many types conforming to different standards, capable of different temperature ranges, with various sizes and accuracies available.

Read More
Technical Learning How to Install a Pressure Tranducer?

How to Install a Pressure Tranducer? OMEGA transducers have three main types of electrical outputs; millivolts (mV), volts (V), and current (mA). It is important for the user to know which output suits his application to ensure proper selection of a transducer.

Read More
Technical Learning Water and Wastewater Test Methods for Operators

Water and Wastewater Test Methods for Operators A variety of test procedures and methods are available for use by water and wastewater operators.

Read More
Technical Learning What is a Voltage Divider?

What is a Voltage Divider? In order to measure a signal which varies over a range greater than the input range of an analog or digital input of a measuring device, a voltage divider can drop the voltage of the input signal to the level the analog or digital input can measure.

Read More
Technical Learning PFA Fluorocarbon Information

PFA Fluorocarbon Information PFA Fluorocarbon Information

Read More
Technical Learning Flow Meter Tutorial

Flow Meter Tutorial So you want to measure flow? The answer would seem to be to purchase a flowmeter.

Read More
Technical Learning Common Problems with Data Acquisition Devices

Common Problems with Data Acquisition Devices Traditional printer drivers are very benign; they are only active, and use the printer port when you tell an application to print.

Read More
Technical Learning Electronic Halogen Leak Detector

Electronic Halogen Leak Detector For many years the most effective, and only, method for finding gas leaks of any type was the use of a soap or bubble solution.

Read More
Technical Learning Industrial pH Monitoring: pH and pH Electrode Basics

Industrial pH Monitoring: pH and pH Electrode Basics pH electrode technology hasn't changed much in the past 50 to 60 years, yet pH electrode manufacturing remains an art.

Read More
Technical Learning Ion Selective Electrodes: Measurement Considerations

Ion Selective Electrodes: Measurement Considerations This article is designed to apply, in general, to all specific ion electrodes.

Read More
Technical Learning What is a Low Pass Filter?

What is a Low Pass Filter? A low pass filter is placed on the signal wires between a signal and an A/D board

Read More
Technical Learning Infrared Quick Help

Infrared Quick Help When to Use Infrared Temperature Measurement

Read More
Product Info Temperature Control Using PID

Temperature Control Using PID Almost every process control application would benefit from PID control.

Read More
Technical Learning Technical Principles of Valves

Technical Principles of Valves Solenoid valves are used wherever fluid flow has to be controlled automatically. They are being used to an increasing degree in the most varied types of plants and equipment.

Read More
Technical Learning Technical Dissolved Oxygen - The Fundamentals

Technical Dissolved Oxygen - The Fundamentals Dissolved oxygen (DO) is the term commonly used in liquid analytical work for the measurement of the amount of oxygen dissolved in a unit volume of water.

Read More
Product Info How Does a PID Controller Work?

How Does a PID Controller Work? As its name implies, a PID controller combines proportional control with additional integral and derivative adjustments which help the unit automatically compensate for changes in the system.

Read More
Technical Learning Contact Closure Inputs: Connect Digital Input & Output DAQ Board

Contact Closure Inputs: Connect Digital Input & Output DAQ Board Many times it is necessary to monitor a contact closure using a PC. Some applications include monitoring a relay closure on a machine to record on-off times, or simply as an alarm to notify someone of an open freezer door.

Read More
Technical Learning Scaling Voltage & Current to Engineering Units

Scaling Voltage & Current to Engineering Units It is very often necessary to convert a voltage, millivot or current reading into a more useful value such as PSI, GPM, LBS, etc.

Read More
Technical Learning Infrared pyrometers

Infrared pyrometers Pyrometer is derived from the Greek root pyro, meaning fire. The term pyrometer was originally used to denote a device capable of measuring temperatures of objects above incandescence, objects bright to the human eye.

Read More
Technical Learning Mechanical Flow meters

Mechanical Flow meters Discussed in this chapter are various types of mechanical flow meters that measure flow using an arrangement of moving parts,

Read More
Technical Learning Differential Pressure Flow meters

Differential Pressure Flow meters The calculation of fluid flow rate by reading the pressure loss across a pipe restriction is perhaps the most commonly used flow measurement technique in industrial applications

Read More
Technical Learning Overview of GPIB protocol

Overview of GPIB protocol IEEE-488 refers to the Institute of Electrical and Electronics Engineers (IEEE) Standard number 488 and is commonly called GPIB (General Purpose Interface Bus).

Read More
Technical Learning RF/Capacitance Level Instrumentation

RF/Capacitance Level Instrumentation Capacitance level detectors are also referred to as radio frequency (RF) or admittance level sensors. They operate in the low MHz radio frequency range, measuring admittance of an alternating current (ac) circuit that varies with level.

Read More
Technical Learning Types of Flow Meters for Different Applications

Types of Flow Meters for Different Applications Measuring the flow of liquids is a critical need in many industrial plants.

Read More
Technical Learning What is a Variable Area Flow Meter?

What is a Variable Area Flow Meter? Variable area flow meters are simple and versatile devices that operate at a relatively constant pressure drop and measure the flow of liquids, gases, and steam.

Read More
Technical Learning Plug-in Cards

Plug-in Cards Although the microprocessor and digital network technologies have fundamentally reinvented the ways in which today's data acquisition systems handle data

Read More
Technical Learning Differential Signal Vs Single-Ended Inputs

Differential Signal Vs Single-Ended Inputs One of the most common questions asked is the difference between single-ended and differential signals inputs, and what applications they should be considered in.

Read More
Technical Learning An Introduction to Venturi Flow Meters, Flow Nozzles, and Segmental Wedge Elements

An Introduction to Venturi Flow Meters, Flow Nozzles, and Segmental Wedge Elements Venturi tubes are available in sizes up to 7 inches and can pass 25 to 50% more flow than an orifice with the same pressure drop

Read More
Technical Learning Pressure sensor

Pressure sensor Piezoelectric presssure sensors can further be classified according to whether the crystal's electrostatic charge, its resistivity, or its resonant frequency electrostatic charge is measured.

Read More
Technical Learning Strain Gauge

Strain Gauge When external forces are applied to a stationary object, stress and strain are the result.

Read More
Technical Learning The RS-232 protocol

The RS-232 protocol Information being transferred between data processing equipment and peripherals is in the form of digital data which is transmitted in either a serial or parallel mode.

Read More
Technical Learning What is an Orifice Plate Flow Meter?

What is an Orifice Plate Flow Meter? The orifice plate flow meter is commonly used in clean liquid, gas, and steam services. It is available for all pipe sizes but it is very cost-effective for measuring flows in larger ones (over 6 inches diameter).

Read More
Technical Learning Wheatstone bridge for strain gauges

Wheatstone bridge for strain gauges In order to measure strain with a bonded resistance strain gauge, it must be connected to an electric circuit that is capable of measuring the minute changes in resistance corresponding to strain.

Read More
Technical Learning An Introduction to Pitot Tubes and Probes

An Introduction to Pitot Tubes and Probes Although the pitot tube is one of the simplest flow sensors, it is used in a wide range of flow measurement applications such as air speed in racing cars and Air Force fighter jets

Read More
Technical Learning What is a thermography?

What is a thermography? Thermography extends the concept of point radiation thermometry to one-dimensional profiles or two-dimensional pictures of non-contact temperature data.

Read More
Technical Learning Strain Gage Technical Data

Strain Gage Technical Data The most universal measuring device for the electrical measurement of mechanical quantities is the strain gage.

Read More
Technical Learning Non-contact thermometers

Non-contact thermometers Historically a radiation non-contact thermometer consisted of an optical system to collect the energy emitted by the target;

Read More
Technical Learning RS485, RS422 and RS232

RS485, RS422 and RS232 Why use RS232 vs RS485 and what is the real difference between RS422 Vs RS485? First, lets define each one. Keep in mind that all three are considered SERIAL, as opposed to IEEE-488 which is PARALLEL.

Read More
Technical Learning pH Control

pH Control Systems pH control systems are characterized by extreme rangeability and sensitivity, and are also subject to difficulties arising from contact between measuring electrodes and hostile fluids.

Read More
Technical Learning Types of level measurement instrumentation

Types of level measurement instrumentation One of the primary principles underlying industrial level measurement is that different materials and different phases of the same material have different densities.

Read More
Technical Learning Specialty Level Switches

Specialty Level Switches Thermal, vibrating, and optical level switches are specialty devices developed to solve specific level detection problems.

Read More
Product Info Working principle of thermocouples

Working principle of thermocouples A typicial thermocouple is made up of two dissimilar metals joined together to form two junctions.

Read More
Technical Learning PLATINUM™ Series PID Control Simulator

PLATINUM™ Series PID Control Simulator In modern industrial systems, temperature is the most common physical measurement...

Read More
Technical Learning Reactive Maintenance vs. Proactive Maintenance: You’re Paying 2-5X More for Maintenance

Reactive Maintenance vs. Proactive Maintenance: You’re Paying 2-5X More for Maintenance Proactive maintenance, reactive maintenance, and the many benefits of switching to proactive maintenance.

Read More
Technical Learning Preventive or predictive: what is the right type of maintenance for your process?

Preventive or predictive: what is the right type of maintenance for your process? Predictive maintenance differs from preventive as it allows you to repair or replace equipment before it runs-to-failure

Read More
Technical Learning Wireless Process Monitoring: Pros & Cons of Using Wireless Devices

Wireless Process Monitoring: Pros & Cons of Using Wireless Devices Wireless monitoring is a versatile and inexpensive solution for a variety of applications in locations with no interference.

Read More
Technical Learning Preventing Explosions with FM Approved Intrinsically Safe Instrumentation

Preventing Explosions with FM Approved Intrinsically Safe Instrumentation Industrial explosions have caused devastating loss of life on many occasions.

Read More
Technical Learning Cellular Monitoring: Process Monitoring with Cellular Technology

Cellular Monitoring: Process Monitoring with Cellular Technology Cellular monitoring is ideal for applications and data logging where updated information is not required in real time.

Read More
Technical Learning New Data Logging, Charting and Alarm Notification System

New Data Logging, Charting and Alarm Notification System The dashboard connects data from your measurement equipments to a webserver for easy-to-use data storage and collection.

Read More
Technical Learning Particle Pollution & Environmental Safety

Particle Pollution & Environmental Safety Indoor air quality is the responsibility of building owners, managers and employers.

Read More
Technical Learning 5 Reasons to Wirelessly Measure Relative Humidity

5 Reasons to Wirelessly Measure Relative Humidity Monitoring Relative Humidity in Lab can be challenging. Choose the most simple and powerful way by using wireless transmitters.

Read More
Technical Learning The Benefits of Implementing Predictive Maintenance

The Benefits of Implementing Predictive Maintenance Predictive maintenance can help you anticipate failure before it happens, saving money, time and making processes more efficient. Learn more about these and other advantages.

Read More
Technical Learning Air Quality Monitoring | Things you should know about it

Air Quality Monitoring | Things you should know about it Ambient air contains life supporting oxygen, nitrogen, carbon dioxide, and chemicals that can harm you and your employees.

Read More
Technical Learning 3 Factors to Consider When Choosing a Custom or Off-the-Shelf Sensor

3 Factors to Consider When Choosing a Custom or Off-the-Shelf Sensor Given the risk to human lives and the financial costs when things go wrong, aerospace engineering...

Read More
Case Study OMEGA Has a Starring Role in the LSST Telescope Mirror

OMEGA Has a Starring Role in the LSST Telescope Mirror The Large Synoptic Survey Telescope (LSST) is a new kind of optical telescope that will view a wider area of night sky than ever before possible. Once operational...

Read More
Technical Learning Ultrasonic Level Sensor Application in Above Ground Bulk Storage Tanks

Ultrasonic Level Sensor Application in Above Ground Bulk Storage Tanks By installing level sensors, operators can be proactive and monitor liquid levels - ensuring environmental regulations associated with the design and operation are consistently met.

Read More
Technical Learning 10 Applications Where You Need a Digital Panel Meter

10 Applications Where You Need a Digital Panel Meter Digital panel meters present numerical information that’s easy to read.

Read More
Technical Learning Infrared Temperature Measurement Theory and Application

Infrared Temperature Measurement Theory and Application Infrared thermometers for non-contact temperature measurement are highly developed sensors which have wide-spread application in...

Read More
Technical Learning What are Nanosensors? How and Where are They Used?

What are Nanosensors? How and Where are They Used? While few engineers need to work at the nano scale, temperature measurement with compact thermocouples is applicable across many fields.

Read More
Technical Learning Differentiating State, Event and Pulse Data Loggers and Defining Applications

Differentiating State, Event and Pulse Data Loggers and Defining Applications Data loggers are instruments that monitor and record changes in conditions over time.

Read More
Technical Learning Sensor Theory of Operation

Sensor Theory of Operation Omega is a reliable source for pressure transducers and load cells that provide high quality data in a myriad of processes.

Read More
Case Study Custom Pressure Transducers

Custom Pressure Transducers A custom pressure transducer is a transducer that converts pressure into an analog electrical signal, often manufactured with the exact specifications required for an application.

Read More
Technical Learning What is MI Cable?

What is MI Cable? The basic construction provides high-temperature capability, exceptional electrical isolation, and physical protection for the conductors especially when subjected to harsh environments.

Read More
Technical Learning PID with Fuzzy Logic Adaptive Control—The Best of Both Worlds

PID with Fuzzy Logic Adaptive Control—The Best of Both Worlds Proportional integral derivative (PID) control is a well established way of driving a system towards a target position or level.

Read More
Technical Learning The importance of wind tunnel testing in the lab

The importance of wind tunnel testing in the lab Failure rates for many electronic components rise with temperature.

Read More
Technical Learning High Temperature Pressure Transducers vs. Cooling Elements

High Temperature Pressure Transducers vs. Cooling Elements Pressure measurement is often a challenging task due to the harsh environments frequently found in industrial manufacturing.

Read More
Product Info Sanitary Sensors

Sanitary Sensors A Sanitary Sensor is a device which measures temperature, flow or pressure in an environment where products will be for human consumption.

Read More
Technical Learning Types of Relays: Mechanical, SSR, Internal or External

Types of Relays: Mechanical, SSR, Internal or External Relays are the control switches that operate with low-powered electrical signals controlling most types of circuits.

Read More
Technical Learning Temperature Measurement in Electromagnetic Environments

Temperature Measurement in Electromagnetic Environments One of the easiest ways to measure and record temperature is with a thermocouple. Thermocouples perform reliably in most environments, tolerating temperature extremes, vibration and even ionizing radiation.

Read More
Product Info M12 Temperature Sensors

M12 Temperature Sensors Temperature sensors provide an input to a system (indicator, controller or other device) that is used to determine the temperature of a specific process or location.

Read More
Technical Learning Doppler Meters Vs Transit Time Ultrasonic Flow Meters

Doppler Meters Vs Transit Time Ultrasonic Flow Meters Ultrasonic flow meters are non-intrusive devices that use acoustic vibrations to measure the flow rate of liquid...

Read More
Product Info Grippers

Grippers A gripper is a motion device that mimics the movements of people, in the case of the gripper, it is the fingers.

Read More
Product Info The Importance of Signal Conditioning

The Importance of Signal Conditioning A signal conditioner is a device that converts one type of electronic signal into a another type of signal. Its primary use is to convert a signal that may be difficult to read by conventional instrumentation into a more easily read format.

Read More
Technical Learning Types of Load Cells

Types of Load Cells Various load cell types are preferred, relative to the needs of the laboratory or operational environment.

Read More
Technical Learning A Brief History of the Temperature Sensor

A Brief History of the Temperature Sensor The sensations of hot and cold are fundamental to the human experience, yet finding ways to measure temperature has challenged many great minds.

Read More
Product Info OEM

OEM Our commitment to maintaining the leading edge through research development and state-of-the art manufacturing keeps OMEGA firmly at the forefront of technology.

Read More
Product Info Strip Heater

Strip Heater A strip heater is a device which is mounted on a surface and used to heat the surface or air (gasses).

Read More
Product Info Calibrator

Calibrator A calibrator is an equipment used to adjust an instrument accuracy, often associated with a specific application.

Read More
Technical Learning What is a Thermal Mass Flow Meter?

What is a Thermal Mass Flow Meter? Thermal mass flow meters measure the mass flowrate of gases and liquids directly.

Read More
Technical Learning Preventing Vibration Damage to Thermocouples and RTD Sensors

Preventing Vibration Damage to Thermocouples and RTD Sensors Challenges presented to temperature measurements in the presence of vibration

Read More
Technical Learning Applications and Benefits of Mineral Insulated Cables in Critical Processes

Applications and Benefits of Mineral Insulated Cables in Critical Processes MI cable is a specialized type of cable used in high temperatures or harsh environmental conditions because it has low flammability, even when operating at high temperatures. It resists oxidation and enables precise measurement.

Read More
Product Info Cryogenic Temperature Sensors

Cryogenic Temperature Sensors Cryogenics is the branch of physics that deals with the production and effects of very low temperatures.

Read More
Product Info Temperature Measurement

Temperature Measurement Temperature can be measured via a diverse array of sensors. All of them infer temperature by sensing some change in a physical characteristic.

Read More
Product Info Wireless Sensors

Wireless Sensors Wireless sensors are standard measurement tools equipped with transmitters to convert signals from process control instruments into a radio transmission.

Read More
Technical Learning Signal Conditioning and Transmission in Temperature Measurement

Signal Conditioning and Transmission in Temperature Measurement Output signals produced by temperature measurement sensors require conditioning to convert them to a form that can be used for further processing.

Read More
Technical Learning Thermowell Characteristics and Selection Criteria

Thermowell Characteristics and Selection Criteria Thermowells are used to guard temperature sensors such as thermocouples, thermistors and bimetal thermometers against damage from excessive pressure, material velocity and corrosion

Read More
Product Info IC Sensors

IC Sensors An IC Temperature Sensor is a two terminal integrated circuit temperature transducer that produces an output current proportional to absolute temperature. The sensor package is small with a low thermal mass and a fast response time

Read More
Product Info Data Acquisition

Data Acquisition In the simplest form, a technician logging the temperature of an oven on a piece of paper is performing data acquisition.

Read More
Technical Learning Understanding Deadband for Pressure Switches

Understanding Deadband for Pressure Switches A pressure switch consists of a sensing component and an electrical switch.

Read More
Technical Learning Lessons about Positive Displacement Flow Meters

Lessons about Positive Displacement Flow Meters Positive Displacement flow meters are the only flow measuring technology to directly measure the volume of fluid that passes though the flow meter.

Read More
Technical Learning How Bright is it? Shining a light on intensity measurement

How Bright is it? Shining a light on intensity measurement Human vision depends on light. Light reflects off surfaces into the eyes, passing through the cornea and pupil to form an image on the retina.

Read More
Technical Learning What is a Cartridge Heater and how does it work?

What is a Cartridge Heater and how does it work? Cartridge heaters are most frequently used for heating metal parts by insertion into drilled holes.

Read More
Product Info Panel Meters

Panel Meters A panel meter is an instrument that displays an input signal in either a digital or analog form.

Read More
Technical Learning What is a Linear Variable Differential Transformer?

What is a Linear Variable Differential Transformer? An LVDT is an electromechanical device used to convert mechanical motion or vibrations, specifically rectilinear motion, into a variable electrical current, voltage or electric signals, and the reverse.

Read More
Product Info Reversible & Non Reversible Temperature Labels & Sensors

Reversible & Non Reversible Temperature Labels & Sensors Temperature labels are temperature monitors consisting of one or more small heat-sensitive indicators sealed under transparent, heat-resistant windows.

Read More
Product Info Infrared Thermometer

Infrared Thermometer On its most basic design an infrared thermometer consists of a lens to focus the infrared (IR) energy on to a detector.

Read More
Technical Learning Air Flow Measurement Instruments: How Precise and Accurate?

Air Flow Measurement Instruments: How Precise and Accurate? Calculating flow rates through ducts, pipes, hoods and stacks (collectively called ducts for our purposes), has never been difficult.

Read More
Product Info Chart Recorders

Chart Recorders A chart recorder is an instrument used to record various process and electrical signals.

Read More
Product Info What is a Temperature Controller?

What is a Temperature Controller? As the name implies, a temperature controller is an instrument used to control temperatures, mainly without extensive operator involvement.

Read More
Product Info What Is A Pressure Transducer?

What Is A Pressure Transducer? A pressure transducer, often called a pressure transmitter, is a transducer that converts pressure into an analog electrical signal. Although there are various types of pressure transducers, one of the most common is the strain-gage base transducer.

Read More
Product Info What is an Ultrasonic Flow Meter?

What is an Ultrasonic Flow Meter? An ultrasonic flow meter (non-intrusive Doppler flow meter) is a volumetric flow meter which requires particulates or bubbles in the flow.

Read More
Product Info What Is A Thermistor And How Does It Work?

What Is A Thermistor And How Does It Work? A thermistor is an element with an electrical resistance that changes in response to temperature.

Read More
Product Info Anemometer

Anemometer An anemometer is an instrument used to measure the speed or velocity of gases either in a contained flow, such as airflow in a duct, or in unconfined flows, such as atmospheric wind.

Read More
Product Info Stepper Motors

Stepper Motors A stepper motor is a brushless, synchronous electric motor that converts digital pulses into mechanical shaft rotation.

Read More
Product Info Strain Gauges

Strain Gauges A Strain gage (sometimes referred to as a Strain Gauge) is a sensor whose resistance varies with applied force; It converts force, pressure, tension, weight, etc., into a change in electrical resistance which can then be measured.

Read More
Product Info How to Measure Acceleration?

How to Measure Acceleration? An accelerometer is a device that measures the vibration, or acceleration of motion of a structure.

Read More
Product Info Flexible Heaters

Flexible Heaters A flexible heater is a device which can conform to the surface which requires heating.

Read More
Case Study pH Meter

pH Meter A pH meter is an instrument used to measure acidity or alkalinity of a solution - also know as pH.

Read More
Technical Learning Understanding What’s Meant by “Intrinsically Safe”

Understanding What’s Meant by “Intrinsically Safe” Fire is a hazard in many industries. Sometimes the risk is quite evident, as when flammable gasses...

Read More
Product Info Data Loggers

Data Loggers Technically speaking, a data logger is any device that can be used to store data.

Read More
Product Info Industrial Heaters

Industrial Heaters Electric heaters are used in a variety of processes where the temperature of an object or process needs to be increased.

Read More
Product Info Level Measurement

Level Measurement Integral to process control in many industries, level measurement sensors fall into two main types. Point level measurement sensors are used to mark a single discrete liquid height–a preset level condition.

Read More
Product Info Thermocouple Wire

Thermocouple Wire Wire that is used in a thermocouple from the point of sensing to the point of cold junction compensation (cjc end) where the signal is measured.

Read More
Product Info What are Electromagnetic Flow Meters?

What are Electromagnetic Flow Meters? A magnetic flow meter (mag flow meter) is a volumetric flow meter which does not have any moving parts and is ideal for wastewater applications or any dirty liquid which is conductive or water based.

Read More
Product Info Immersion Heater

Immersion Heater An immersion heater is a device which is installed in a tank or container to heat a liquid. The installation can be over-the-side, flanged or threaded.

Read More
Product Info What is a Pressure Gauge?

What is a Pressure Gauge? Pressure gauges are among the most often used instruments in a plant. But because of their great numbers, attention to maintenance--and reliability--can be compromised.

Read More
en-US
en
Save Configuration