What is IIoT?

IIoT is the internet of things implemented in industries. However, it is not as simple as the definition. The IoT that we know and understand is primarily designed around the requirements of our home. IIoT is for largescale industries, and they have precise requirements. The reason why IIoT even exists is that it brings in many advantages or features that regular IoT doesn’t.

For a long time, industries were not at the forefront of the digital revolution. And there is a valid reason for this because, in industries, large scale changes are often risky and can create massive losses to the company if it doesn’t work out. Hence a “resistance to change” is often seen in industries when we propose a new technology to them. IIoT has also seen such responses during its initial rollout.

Omega Link Smart Gateway | Product Highlight

What is Edge Computing?

The concept of edge computing has been around for several years, stemming from the days of on-premise Computer Instrumentation or Human Machine Interface (HMI) computers. In the advent of the Industrial Internet of Things (IIoT), it has quickly transformed from instrumentation to a much more powerful computational device.

As the name implies, edge computing is deployed on-premise or “edge” of cloud computing where data is generated in its native format. This novel approach allows data to be collected, analyzed and synchronized with one or more edge computing devices. It can then make a local decision of process and storage before sending only relevant data up to the cloud for further complex computation such as A.i and other mathematical modeling.

In essence, edge computing improves reliability and performance locally without delay associated with round trip communication delay from the internet. This is of critical importance when the process and data sampling time are measured down to milliseconds instead of seconds.

Learn More

How will it affect bussinesses?

Smart sensors are effective when employed in production control and management. These devices allow manufacturing businesses to monitor various parts of the work environment. For example, sensors are useful to measure a variety of physical quantities from the operating temperature of machines to the rpm of a rotating component.

Through continuous monitoring of these parameters, it is possible to detect anomalies in production processes, identify ways to improve operating efficiency, and also prevent hazardous situations in the work environment. Smart sensors can also work as triggers for alarms to control and protect the equipment as well as the workforce interacting with it.

However, production is not the only area that can benefit from smart sensors. Here are other processes and workflows that businesses can optimize through these smart sensing devices.

  1. Supply Chain Optimization
  2. Better Machine and Equipment Utilization
  3. Continuous Monitoring of Processes for Better Quality and Worker Safety
  4. Connected Buildings


Learn More

OMEGA products used in this application

Omega Link Long Range Wireless/Modbus IIoT Ethernet Gateways
Omega Link Long Range Wireless/Modbus IIoT Ethernet Gateways
Omega Link Wireless IIoT Smart Environmental Sensors
Omega Link Wireless IIoT Smart Environmental Sensors
Omega Link M12 Modular Thermocouple and RTD Temperature Smart Probe
Omega Link M12 Modular Thermocouple and RTD Temperature Smart Probe
Omega Link M12 Modular Environmental Monitoring Smart Probes
Omega Link M12 Modular Environmental Monitoring Smart Probes
Benefits of Remote Monitoring Using IIoT

Some benefits can be in the form of:

  1. Centralized monitoring
  2. Accurate monitoring
  3. Improved team efficiency
  4. Faster response to incidents
  5. Compliance to regulatory requirementsli>
  6. Business continuity in the event of disasters
  7. Lower operating costs


Learn more

Real-World Examples of IIoT in Action

IIoT can bring significant benefits to industries and companies that understood their importance have already implanted the technology and are reaping the rewards.



  1. IoT Solution in Automation and Food Safety
  2. Alarmed Freezer Door
  3. Monitor Asphalt Temperature
  4. Other IIoT examples

Related articles