Skip to search Skip to main content Skip to navigation

Attention Microsoft Edge Users: the Edge browser is experiencing technical difficulties. Please clear your cache and make sure you are on the most recent version. Alternatively, Chrome is a preferred browser.

We noticed you are from . Visit your local site for regional offers and live support.

Get Curious. Get Going.

Ready to become an expert? Dive into our most popular videos and resources articles below.

Browse our most popular articles
Strip Heater What Is A Strip Heater And What Is It Used For?

A strip heater is a device which is mounted on a surface and used to heat the surface or air (gasses).

What is a Cartridge Heater and how does it work? What Is A Cartridge Heater And What Is Used For? – Omega Engineering

Cartridge heaters are most frequently used for heating metal parts by insertion into drilled holes.

Industrial Heaters what is an industrial electric heater?

Electric heaters are used in a variety of processes where the temperature of an object or process needs to be increased.

Everything you need to know about Immersion Heaters Everything you need to know about Immersion Heaters

An immersion heater is a device which is installed in a tank or container to heat a liquid. The installation can be over-the-side, flanged, or threaded.

An Introduction to Flow Meters An Introduction to Flow Meters

As the name implies a Flow meter is an instrument for monitoring, measuring, or recording the rate of flow, pressure, or discharge of liquids or gasses.

What is an Ultrasonic Flow Meter? What is an Ultrasonic Flow Meter?

An ultrasonic flow meter (non-intrusive Doppler flow meter) is a volumetric flow meter which requires particulates or bubbles in the flow.

What are Electromagnetic Flow Meters? What are Electromagnetic Flow Meters?

A magnetic flow meter (mag flow meter) is a volumetric flow meter which does not have any moving parts and is ideal for wastewater applications or any dirty liquid which is conductive or water based.

What is a Coriolis Flow Meter and How Does it Work? What Is A Coriolis Flow Meter and How Does It Work

A Coriolis flow meter is a type of mass flow meter. It is designed differently and works differently than thermal or differential mass flow meters.

Strain Gauges Strain Gauges, How does it work?

A Strain gage (sometimes referred to as a Strain Gauge) is a sensor whose resistance varies with applied force; It converts force, pressure, tension, weight, etc., into a change in electrical resistance which can then be measured.

What is a Linear Variable Differential Transformer? What is a LVDT Sensor?

An LVDT is an electromechanical device used to convert mechanical motion or vibrations, specifically rectilinear motion, into a variable electrical current, voltage or electric signals, and the reverse.

Installing a Load Cell: Best Practices Installing a Load Cell. How to mount and connect a load cell?

Each load cell installation is unique. Consult a structural engineer when your application requires very high accuracy, long-term stability, custom specifications, or when using in a varied R&D environment.

Blog Setting the Standard

Setting the Standard When it comes to temperature measurement in an important application process – like yours – precision is paramount. So much relies on the accuracy of these measurements, and the quality of the instrumentation and devices that are used can make all the difference. We put our Super OmegaClad XL and our standard Inconel probes up against some of our competitors’ similarly spec’d probes in a battery of long-term product testing – and the results speak for themselves.

Read More
Technical Learning Ultrasonic Level Sensors in Action

Ultrasonic Level Sensors in Action By installing level sensors, operators can be proactive and monitor liquid levels - ensuring environmental regulations associated with the design and operation are consistently met.

Read More
Video

Discover the Different Types of Pressure Measurement Discover the different types of pressure measurement and the differences between them. This video, which features one of our star engineers, provides a comprehensive overview to elevate your understanding.

Read More
Blog Fine-Tuning the Noise

Fine-Tuning the Noise A signal conditioner is a device that converts one type of electronic signal into a another type of signal. Its primary use is to convert a signal that may be difficult to read by conventional instrumentation into a more easily read format.

Read More
Blog Digital Panel Meters

Digital Panel Meters Accurate measurement of electrical parameters is crucial for efficient operation and safety across a wide range of applications. Digital panel meters, which provide a precise, real-time display of vital electrical quantities – such as voltage, current, resistance, frequency, strain, and temperature – can assist in achieving this high level of accuracy. These devices offer a user-friendly interface with clear numerical displays – eliminating the guesswork that often accompanies analog meters and allowing operators to monitor system performance at a glance.

Read More
Technical Learning Fluid Dynamics

Fluid Dynamics Measuring and monitoring fluid levels accurately and precisely requires choosing the correct methodology for the target medium and vessel.

Read More
Blog Brewing Up Precision

Brewing Up Precision In this application, the purpose is to measure the temperature of the motor in an industrial coffee grinder during the grinding process to better understand the strain on the motor.

Read More
Technical Learning IIoT and Small Businesses: A Match Made in the Cloud

IIoT and Small Businesses: A Match Made in the Cloud Operational efficiency is key to the success of any small business, and IIoT essentially helps you achieve that by turning your offline processes to online through a connected environment.

Read More
en-US
en
Save Configuration